Oriental Motor U.S.A. Corp.

Modular Automation

Modular Automation

Solutions that Allow the Assembly of Small or Varying Lots with Modular Automation Compatible Products

  • Flexibility in Production Layout
  • Productivity Improvements
  • High-Mix, Low-Volume Production
  • Resolve Labor Shortages
  • Space Saving
  • Energy Saving

 

Modular Concept

The key to Modular Automation is the realization of the "Flexibility within the Production Line Layout". Modular Automation products support the next generation of automation.

Today’s challenge is to create flexible and reliable manufacturing lines to meet tomorrow’s manufacturing requirements. To achieve this, more and more companies are working on modularization, which allows the line configuration to be rearranged according to the situation.

As an increasing number of manufacturing locations are working on automation to replace common tasks, such as transporting materials, assembling products and performing work in difficult-to-access areas, Modular Automation compatible products are a group of products designed to support this direction.


Introducing the Concept of Modular Automation

Modular automation is the next phase of factory automation where the same production line is separated into modules and can be quickly reconfigured to adapt to different needs. This video illustrates the new rapidly expanding form of automation and how traditional assembly lines are transformed into modular assembly lines. Modular automation compatible products by Oriental Motor include the compact and lightweight DC-powered products, such as the AZ Series mini driver and the BLV Series R Type.

 

Example: Work Transportation Robots Between Each Process

By converting the conveyors that are part of a production line to mobile robots, flexible configuration of the line becomes possible, and a more efficient production line is realized. A robot with a small turning radius can move and work even in a limited space. It is effective as a means to improve efficiency.

Example: Flexible Modified Module Line Adapted to the Production

By modularizing the equipment for each process, flexible layout changes can be implemented according to the product. In order to realize modularization, it is necessary to unify the equipment with certain standard sizes and simplify the power supply wiring. Since these modular sections are designed to move on their own, it is also necessary to consider making the device lighter and more compact. In the near future, there may come an era in which all production equipment will be self-propelled by battery drive, and layout changes will be made by AI on an efficient movement route.

 

 

Additional Examples:


 

Modular Automation Compatible Products

Modular Automation Products are a group of products that share the common features of being battery-powered, compact and lightweight. Optimized for use in self-propelled devices and mobile equipment, they contribute to the realization of flexible automation lines and mobile automation.

αSTEP AZ Series mini Driver for Motors & Actuators

αSTEP is now equipped with a newly developed absolute mechanical encoder, no back up battery required. The AZ Series mini driver has been designed to be compact and lightweight, freeing up valuable cabinet space. Combine it with the wide product selection of the AZ Series.

mini Driver

Driver

Motor Types

Power Supply

mini Driver

AZ Series mini Drivers

Closed Loop, Absolute Encoder AZ Series Stepper Motors

24/48 VDC

MRC Robot Controller

The MRC01 robot controller supports easy programming and control of in-house designed custom built robots with 3 simple steps: "Initial Setup", "Operating Programming" and "Operational Checking".


Brushless DC Motors BLV Series R Type

Redesigned, compact driver and motor. Slow speed, 1 rpm up to 4,000 rpm. Designed to support battery-powered applications.

Brushless DC Motors

Series

Output Power

Power Supply

100 W Brushless DC Motors

BLV Series R Type Brushless DC Motors

Electromagnetic Brake

24 - 48 VDC

Brushless DC Motor Application

Applications

For Example, These Motors & Drivers can Contribute to Flexibility within the Production Line Layout

Examples


Case Study - Real world example of modular automation that increases productivity utilizing an internally assembled robot

Assembly Line Robot

Oriental Motor, a global manufacturer of fractional horsepower motors, supports the internal designing of application-specific robots with the AZ Series. The AZ Series is a family of motors, actuators, and network drives that feature an absolute sensor, closed-loop control, and easily works with the multi-axis MRC0l controller. This combination of products allows for internally designed and built in-house automation that are designed according to the circumstances and decrease the hurdles in locations where automation wasn't possible; for example, where commercial robots had space restrictions or lack of space inside the equipment, cost limitations, and other barriers.

Below is an example of in-house automation built using these AZ Series products.

Automated Sensor Line Assembly Robot

The two actions of transportation between neighboring process equipment and additional positioning have been combined in one horizontal SCARA robot, reducing the processes in order to deal with the issue of restricted equipment width and height as production lines are modularized O.

This robot is arranged beside the production robot. By having the transportation work performed by the production robot and the parts settling work performed by the internal manufacturing robot carried out at the same time, the overall machine time is reduced f). The robot has a simple and compact design comprised of the following, with one unit costing around $8,000 (including the electrical components): an AZ series DC-input motor, a DGII series hollow rotary actuator, a DR series compact linear actuator, an EH series electric gripper, and an MRC01 robot controller. Although there were initially some concerns about how to control and set a multi-axis robot, even inexperienced users were able to make the settings smoothly using the MRC Studio programming software 8.

Contact the Oriental Motor Customer Support Center for details and the selections available.

Assembly Line Robot

Robot Controller


Engineering Notes
We're Here to Help

Service and Support

 

Business Hours:

Monday to Friday

8:30am EST to 5:00pm PST

 

Sales & Customer Service:

1-800-418-7903

Technical Support:

1-800-468-3982



©2026 - ORIENTAL MOTOR USA CORP. - All Rights Reserved