Oriental Motor U.S.A. Corp.


Mobile Robot ControllerMobile Robot Controller

MVC01 Mobile Robot Controller

The MVC Mobile Robot Controller is equipped with a driving control function for AGV/AMR transport robots.

  • Support from start-up to maintenance with dedicated PC software
  • Output gyro odometry with built-in IMU
  • Compatible with BLV Series R Type Brushless DC Motor


Robot Controller Lineup

Item

Network

Power Supply

Robot Controller

MVC01
Mobile Robot Controller

RS-485

24 ~ 48 VDC

Controller for Transfer Robot Useful for In-House Production and Development of AGVs/AMRs

In the in-house production and development of AGVs/AMRs, it is usually necessary to implement kinematics corresponding to the robot's wheel structure. It is necessary to distribute speed to each motor according to the respective mechanism, such as differential drive or mecanum wheels, a factor that has complicated the development of higher-level software.

The MVC01 internally processes these differences in movement mechanisms, allowing the robot to be controlled from a host controller using only simple speed commands.

Supported Speed Command

  • Forward Translational Speed
  • Lateral Translational Speed*
  • Rotation Speed

*Only for robot types capable of moving in all directions, such as those with mecanum wheels.

 


Compatible Products

Brushless DC Motor BLV Series R Type

Compatible Products

Its compact size fits even in tight spaces. It is equivalent in size to the BLV Series R type driver.

Mobile Robot Controller
Mass: 60 g


BLV Series R Type Driver
Mass: 120 g



Reduces the Burden of Software Development by Sharing the Role With Host Controllers

Mobile robot controllers are equipped with travel control functions necessary for AGV/AMR driving. The mobile robot controller performs calculations for each wheel and control of synchronous between axes, thus reducing the burden of software development and start-up time.

Modularized Travel Control Functions for Transfer Robot (AGV/AMR)

Controlled by Host Controllers Only

Controlled by "Host Controllers + Mobile Robot Controller"

Host controllers are responsible for both host application and travel control application

[Role sharing]
・Travel control application → mobile robot controller in charge
・Host application → host controller in charge

Large software design burden

Small software design burden

Component Comparison (For AMR)

Component Comparison (For AMR)

Application Comparison (For AMR)

Application Comparison (For AMR)

Improved Customizability of Wheels, Drive Systems, etc. Through Modularization of Travel Control Functions

If all software is developed in ROS, the ROS program must be changed when the mechanism is customized, such as when wheels are changed, which increases the burden of updating. By using the MVC01 for travel control, wheel mechanism settings can be performed in MVC Studio, so wheel management on the host side is unnecessary. As a result, modifications to the host program can be kept to a minimum even when the mechanism is changed.

To Change the Wheel Configuration, Robot Size, etc., Simply Reconfigure MVC01

Slip Detection Through Accurate Position Information Acquisition by IMU

With a built-in IMU, the mobile robot controller can output position information calculated by gyro odometry. Gyro odometry is a method of estimating position information from the encoder data of the IMU and motor. When moving on uneven terrain, slippage can easily cause errors in the actual robot and position information, but the IMU can output more accurate position information.

 

Inertial Measurement Unit (IMU)

A sensor that combines an acceleration sensor and a gyro sensor. Detects 3-dimensional inertia motion (Translational and rotational motion of three cartesian directions).


Free Support Software MVC Studio

Software that supports from start-up to maintenance of the mobile robot controller is available. In addition to setting and editing various parameters, various statuses can be monitored. The software is available for free download.

Follow the Guidance to Complete Initial Settings Without Getting Lost

A series of initial settings, such as selection of drive system (2-wheel drive, 4-wheel drive, etc.) and input of mechanism information, can be performed in a wizard format. By following the guidance and illustrated instructions, even first-time users can complete the settings in a short time.


Follow the Steps to Set Up

Follow the wizard menu to proceed with the initial settings of the robot.

[1] Selection of Robot Type

Select 2-wheel drive or 4-wheel drive

MRC Easy GUI Programming


[2] Axis Setting

Set gear ratio and rotation direction for each axis

Axis Setting


[3] Robot Information Settings

Set robot mechanism information

Robot Information Settings


[4] Calibration

Calibrate the IMU

Calibration


[5] Operation Check

Perform test operation

Calibration



 

Parameter Setting and Monitoring Function for Start-Up and Maintenance

Parameter Setting

The configured data can be saved on a PC so that the same settings can be used even if the controller is replaced.

Robot Information Settings


Monitoring Function

Robot position, speed, I/O signals, alarms, etc. can be monitored.

Calibration



ROS 2 Compatibility

ROS 2 (Robot Operating System 2) is an open-source middleware framework for robot development. Using ROS 2 allows complex controls to be built easily and offers benefits such as highly reliable communication and real-time support. It can also be utilized in a wide range of fields, such as industrial robots, inter-process transfer robots, and service robots. MVC01 supports ROS 2.

You can download the following ROS nodes, manuals, and sample code.

  • Create and submit queries
  • Receiving a response
  • Data distribution

Please provide your own ROS unit and the necessary adapter cables for connecting it to your PC. This document is intended for individuals with expertise in ROS and Linux. Support is not provided for inquiries regarding ROS installation, usage, or Linux. Some of our products include electric actuators that are integrated into the series.


In-House Production Case Studies

In-House Production Case Study of AGV (Automated Guided Vehicle) – Automation of Manual Handling Processes

We developed the AGV in-house, aiming for inline automation. We were able to reduce system development costs compared to off-the-shelf products.


Example of a Transfer Robot built using ROS 2

We will introduce an example of a transfer robot in operation built using ROS 2.

Self-Navigation

Line Tracing

Manual Operation

Features

Performs self-navigation by estimating its position based on factory maps.
Capable of transporting items to a destination while avoiding obstacles.

Recognizes vinyl tape on the floor with a camera and travels steadily along a set route.

Drives via remote control from a smartphone/tablet app. Supports flexible operations, such as prototyping and operation checks.

Implementation Costs

High

Low to medium

Low to medium

Suitable Environments and Applications

• High-mix, low-volume production
• Factories with frequent layout changes
• Collaborative environments with humans

• Long-distance, heavy-load transport
• Fixed transport routes
• Organized environments

• Prototype line
• Environments requiring flexible operation

Self-Navigation

Self-navigation to the destination while avoiding obstacles


Line Tracing

Stable travel along floor lines


Manual Operation

Remote driving via app operation


Comparison of System Configurations

Comparison of System Configurations


I/O Cables

Driver Cable

It is a general-purpose multi-core cable convenient for connection between the driver and host controller.

Item

Lead Wires

Length

CC06D005B-1

6

0.5 m (1.65 ft.)

CC06D010B-1

1 m (3.3 ft.)

CC06D015B-1

1.5 m (4.9 ft.)

CC06D020B-1

2 m (6.6 ft.)

CC10D005B-1

10

0.5 m (1.65 ft.)

CC10D010B-1

1 m (3.3 ft.)

CC10D015B-1

1.5 m (4.9 ft.)

CC10D020B-1

2 m (6.6 ft.)

CC12D005B-1

12

0.5 m (1.65 ft.)

CC12D010B-1

1 m (3.3 ft.)

CC12D015B-1

1.5 m (4.9 ft.)

CC12D020B-1

2 m (6.6 ft.)

CC16D005B-1

16

0.5 m (1.65 ft.)

CC16D010B-1

1 m (3.3 ft.)

CC16D015B-1

1.5 m (4.9 ft.)

CC16D020B-1

2 m (6.6 ft.)


MVC Studio Software

MVC Studio logo

The MVC Studio software supports users with everything for the mobile robot controller MVC01 from start-up to maintenance. In addition to setting and editing various parameters, various statuses can be monitored.


 

Accesories

EPCR1201-2, CR Circuit for Surge Suppression

CR Circuit for Surge Suppression


 


System Configuration

System Configuration


CAD / Manual Search

To locate product CAD and Operator Manuals please search using the product Item Number.

Downloads




©2026 - ORIENTAL MOTOR USA CORP. - All Rights Reserved