Oriental Motor U.S.A. Corp.

Case Study - SCARA Robots Motor Assembly Demo

For this case study, our application engineering group combined 2 OVR Series SCARA robots and MRCU robot controllers with EZS & KR Linear Slides and EH Series Electric Grippers for end effectors to demonstrate picking and placing coordination in a tight workspace assembling a stepper motor.

 


Area Outputs

Setting Workplace Zones to Avoid Collisions

The MRC controller allows 2 types of area outputs:

1) Area[]

2) Area[]-AX

In this demo, these area outputs are combined to divide the entire workspace into 4 zones (shown below).

Each robot can avoid collisions by entering a zone only after confirming that no other robots are present.


Area Outputs

Area Output

These output set how the controller operates when the command position of the TCP enters the user-defined area.

AREA0 to AREA4 outputs: The AREA output is turned ON when the command position of the TCP is within the range set in the “User-defined area” parameter.

It is turned ON when the command position of the TCP is within the range of the user-defined area even while the robot stops.

AREA0-AX to AREA2-AX outputs: When the axis position selected with the “AREA-AX target axis selection” parameter is within the range set with the “AREA-AX positive direction position” parameter or “AREA-AX negative direction position” parameter, the output signal of the corresponding axis is turned ON. It is turned ON even if operation is stopped.

In this demonstration two SCARA robots are working together. The AREA output allow the other robot to know where the TCP of the robot present.

Using the “WAIT (Signal)” command before the robot enters that area will help prevent collisions.


MRC Studio Command Setting

Area Outpur Command

MRC Studio Parameter Setting

Parameter Setting

MRC Studio Area0 Range Setting

Area0 Range Setting

MRC Studio Area0-AZ Range Setting

Area0-AX Range Setting

 

Learn More About The Products Used

OVR Series SCARA Robots

SCARA Robots

 

MRCU Integrated Robot Controller & Drivers

Integrated Robot Controller & Drivers

 

MRC Studio Robot Software


 

MRC Studio

 

 

EH Series Gripper

Electric Gripper

 

EZS Series Linear Slides

EZS Series Linear Slides

 

AZ Series Step-Servo Motors

AZ Series Stepper Motor

 

THK Linear Slides

THK Linear Slide

 

 

 

 

 

We're Here to Help

Service and Support

 

Business Hours:

Monday to Friday

8:30am EST to 5:00pm PST

 

Robot Support:

1-800-443-0775

 

On Demand Webinar
Industrial Robots



©2026 - ORIENTAL MOTOR USA CORP. - All Rights Reserved