Oriental Motor U.S.A. Corp.

Case Study - SCARA Robots Motor Assembly Demo

For this case study, our application engineering group combined 2 OVR Series SCARA robots and MRCU robot controllers with EZS & KR Linear Slides and EH Series Electric Grippers for end effectors to demonstrate picking and placing coordination in a tight workspace assembling a stepper motor.

 


Tool Offset

Changing Tool Offset Command

The MRC controller allows 2 Tool-Offset settings of TCP can be set to program different shape or position being used.

In this demo, the TCP position is switched between the Electrical gripper and the Pneumatical suction cap.

In this demonstration, OVR3041K3-H uses two end effectors, EH electrical gripper and CKD puematic suction cup.

The EH electrical gripper handle the rotors and the pneumatic suction cup handles the stators.


Changing tool offset: This is a command to switch the tool offset. Two offset values of TCP can be set to the controller according to the shape of the tool being used. When using two tools with different shapes, TCP can be switched according to the tool being controlled.

Tool Offset

MRC Studio Command Setting

Tool Offset Command Setting

MRC Studio Tool Offset Parameter Setting

Setting Parameter
Tool Offsets

 

Learn More About The Products Used

OVR Series SCARA Robots

SCARA Robots

 

MRCU Integrated Robot Controller & Drivers

Integrated Robot Controller & Drivers

 

MRC Studio Robot Software


 

MRC Studio

 

 

EH Series Gripper

Electric Gripper

 

EZS Series Linear Slides

EZS Series Linear Slides

 

AZ Series Step-Servo Motors

AZ Series Stepper Motor

 

THK Linear Slides

THK Linear Slide

 

 

 

 

 

We're Here to Help

Service and Support

 

Business Hours:

Monday to Friday

8:30am EST to 5:00pm PST

 

Robot Support:

1-800-443-0775

 

On Demand Webinar
Industrial Robots



©2026 - ORIENTAL MOTOR USA CORP. - All Rights Reserved