For this case study, our application engineering group combined 2 OVR Series SCARA robots and MRCU robot controllers with EZS & KR Linear Slides and EH Series Electric Grippers for end effectors to demonstrate picking and placing coordination in a tight workspace assembling a stepper motor.

This allow users to predefine up to 16 position points (Point Data 0 to 15), with coordinates such as X, Y, Z, Rx, Ry, and Rz, and then call those points directly from motion commands instead of manually entering coordinates every time.
In this demo, data points are set for the (1) Stator, (2) Rotor, (4) Flange.


The MRC controller has two types of WAIT Commands; WAIT time and WAIT signal.
Wait (time): The next command is executed after the specified wait time has elapsed.
Wait (signal): The next command is executed after the specified signal satisfies the waiting end condition (ON or OFF).
In this demonstration, the WAIT (time) is used before and after the pneumatic suction to provide a buffer allow the suction cup securely engaged with the stator.
The WAIT (signal) is used for a couple different purpose, such as waiting the other SCARA to move out from the AREAs and WAIT for the other SCARA to complete sudden command to timing synchronized motions.



MRC01 has 8 Programmable Direct Inputs and 8 Programmable Direct Outputs.
Direct outputs can be used to control external driver/controller of additional axes and device. In this demonstration, the CKD pneumatic valve and AZM24AK-CSF8-50 are controlled by using the Programmable Direct outputs.


MRC01 has four Virtual inputs.
Virtual Inputs (VIR-IN0 to VIR-IN3) are internal software-based input signals within the MRC01 controller. Unlike physical I/O points, they do not require any external wiring or input terminals. They can be configured and used internally to trigger robot functions, logic, or control sequences.



OVR Series SCARA Robots
|
MRCU Integrated Robot Controller & Drivers
|
MRC Studio Robot Software
|
EH Series Gripper
|
EZS Series Linear Slides
|
AZ Series Step-Servo Motors
|
THK Linear Slides
|
|